Before Installing

Before installing CSense 2024, ensure that the following requirements are met:

  • Ensure that your environment meets the minimum hardware and software requirements for Proficy CSense. 

    NOTE: The CSense installer must be run from your machine's local drive. Installing CSense from a network drive or network folder is not supported.

  • The Windows accounts you specify for the CSense Services must have the Log On as a Service right on the local machine.

  • Consider disabling virus-checking software and Internet security applications on your system for the duration of the installation process. These applications may impact on the installation process or cause it to appear unresponsive.


Related topics:

  

CSense 2024- Last updated: June 20,2025